What is the dynamic range of the ADA4350 when used as a TIA?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the dynamic range of the ADA4350 when used as a TIA?

 

It can be as big as you want it to be. However, if you use a large resistive
load at the TIA output and a small feedback resistor, a series RC circuit may
be needed at the output of the TIA to clamp down the peaking. For details,
please refer to the section “The Effect of Low Feedback Resistor Rfx” on the
ADA4350 datasheet.  If you use a large feedback resistor (> 1MOhm), you may
consider using a T-network configuration to maximize your signal bandwidth.
Please see the  section  “Using the T network to implement large
feedback resistor values” in the ADA4350 datasheet.

Attachments

    Outcomes