What ADC can I pair with the ADA4350? Can I use the ADC driver in other gain configurations?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What ADC can I pair with the ADA4350? Can I use the ADC driver in other gain
configurations?

 

The ADA4350 is designed to work with precision converters up to 16 bit. As for
the speed of the  precision ADC, it depends on the ENOB requirement of
the customer. In general, the higher the  input frequency, the lower the
ENOB. The ADC driver can be configured in other gain  configurations.
Please use the connection diagram below as a reference.

Attachments

    Outcomes