ADA4096: ESD ratings

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Could you please send me the ESD ratings of the inputs of the ADA4096 opamp,
which we use in the input stage of a pt100 sensor




 

The ADA4096-2 passed ±2500V Human Body Model (HBM), ESD Class 2 (ESD Test
Specification ESDA/JEDEC JS-001-2011) .
The ADA4096-4 passed ±2000V Human Body Model (HBM), ESD Class 2 (ESD Test
Specification ESDA/JEDEC JS-001-2011) .

Kindly find more information concerning ESD models and testing, causes for ESD,
failure mechanisms and how-to-avoid ESD in the tutorial MT-092 here

http://www.analog.com/static/imported-files/tutorials/MT-092.pdf

and in more detail in section "Electrical Overstress" in the Reliability
Handbook UG-311 here

http://www.analog.com/static/imported-files/user_guides/UG-311.pdf .

I hope this helps, if you have any further questions do not hesitate to contact
me.




Attachments

    Outcomes