ADA4077-2 Drop-In Replacement

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is ADA4077-2 a drop in replacement for the previous generation?

 

Almost all specifications of this newer product are improved over the parts in
older generations. Exceptions are IVR and output swings which are slightly
different. The IVR and swings values for  ADA4077-2 are −13.8<IVR<+13 and
-13.5<Vout<14.1V while these are -13.5V<IVR<13.5V and -14V<Vout<14V for OP2177
as an example. Please note that IVR does not extend on the positive side and
the part does not swing as close to the negative rail.
1 person found this helpful

Attachments

    Outcomes