AD9889B: does the AD9889B support the format 1080i50

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I wanted to know if AD9889B supports the Video Format 1080i-50?


Yes, the AD9889B does support 1080i50. As long as a format is within the
maximum clock range (150MHz), then it can be supported. There is nothing that
is specific to the support of a given mode. Although we do not specifically
address VESA graphics modes, they are also supported in all forms through the