AD9838 Datasheet error: Absolute maximum ratings for AVDD to DVDD

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

The datasheet states on the frontpage that avdd can be 5v while dvdd is 3V.
Absolute max. Ratings state that avdd to dvdd should be -0.3V to 0.3v. Which is
true

 

There is an error in the absolute maximum ratings, the -0.3V to 0.3v
restriction on AVDD to DVDD should not be there and will be removed in next
revision of the datasheet.

Attachments

    Outcomes