AD9767: Load range

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

If I increase the output load resistors, what is the maximum output voltage
that can be guaranteed?

 

IOUTFS is in the range of 2mA to 20mA and the voltage IOUTAx and IOUTBx needs
to be kept within the compliance range -1.0V to +1.25V. Therewith the applied
load needs to stay in range 1.25V/20mA to 1.25V/2mA = 62.5 Ohm to 625 Ohm. In
this load range the part stays into specified output range, and 1.25V output
can be delivered.

Attachments

    Outcomes