What is the expected AC performance of the AD9684 at high input frequencies?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the expected AC performance of the AD9684 at high input frequencies?

 

The AD9684 provides best in class AC performance for signals up to 2GHz. At
frequencies above  1GHz, the input signal can be run at -3dBFS instead of
-1dBFS to achieve better SFDR  performance without paying any penalty on SNR.

Attachments

    Outcomes