Should I connect to ground the CMLI, CMLQ, FSADJI and FSADJQ pins?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Should I connect to ground the CMLI, CMLQ, FSADJI and FSADJQ pins?

I'm setting the following AD9716 registers with the following values?
Reg    Bin    Hex
0x04 10000000 80
0x05 00000000 00
0x07 10000000 80
0x08 00000000 00

 

From your register settings IRseten=1, QRseten=1 and IRcmlen=QRcmlen=0. This
means:

CMLI and CMLQ should be connected to AVss via a 0ohm resistor.

FSADJQ and FSADJI are set as the outputs of the Auxillary DACs. Then you will
need to set the AUXDACQ, AUXDACI, AUXCTLQ, and AUXCTLI registers accordingly.
More on the Auxillary DACs can be found on page 49 of the datasheet:


The latest datasheet can be found at the following ADI link:
http://www.analog.com/static/imported-files/data_sheets/AD9714_9715_9716_9717.pd
f

Attachments

    Outcomes