Can the AD9684 support DC coupled signals?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can the AD9684 support DC coupled signals?

 

The AD9684 can support DC coupling if the common mode voltage is kept at the
recommended  level. In DC-coupled applications, set the common-mode voltage to
2.05 V, ±100 mV to ensure  proper ADC operation. The full-scale voltage setting
must be at a 1.7 V p-p differential if running  in a DC-coupled application.

Attachments

    Outcomes