AD9510: Evaluation PCB

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

1 . Is the output for the external low pass filter a current or a voltage? 
2. How is the maximum and minum voltage that can be presented in reference and
3. RcPSet in my case is 5.1 Kohm how can i change it?


Question 1:
This is a Voltage ouput with a 100ohm Load.

Question 2:
The balum is a 1:1  balumn , therefore the spec's in the datasheet hold for
this input - which is 150mV input range, as the Device is selfbiased.

Question 3:
See datasheet page 50 = CP_lsb = 3.06/CPRset - This is all you need to insert
your own CPRset.