Baking the AD9951A

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Does this part have to be baked 24hours prior soldering it.


Only packages which exceed the recommended storage conditions should be baked
before reflow soldering. The AD9951 has a Moisture Sensitivity Level rating of
3. If the part is removed from the drypack environment,
its shelf life is 1 week before which it must be soldered or resealed in a
drypack. Beyond this time it needs rebaking (125C +/- 5C/24 hours) as per the
Jedec standard J-STD-20.