Is there a solution to use the AD9272-65EBZ using the FMC interposer board?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is there a solution to use the AD9272-65EBZ using the FMC interposer board?

 

The connector on the AD9272 evaluation board is compatible with the
HSC-ADC-EVALCZ.  However, there is an interposer to translate to the Xilinx
FPGA kits.  There is a wiki page on the solution: 

http://wiki.analog.com/resources/fpga/xilinx/interposer/ad9279

Even though this references the AD9279, the interface with the AD9272 is
identical.  The FMC interposer board can be ordered via SAP.

Attachments

    Outcomes