Highest input clock frequency supported by the AD9250

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the highest input clock frequency supported by the AD9250?

 

The maximum Nyquist input clock frequency is 625MHz and a maximum RF input
clock frequency is 1500MHz but the maximum sampling rate is 250Msps.  The
AD9250 supports a clock divider function (up to divisible by 8 for the Nyquist
clock and divisible by 4 for the RF clock) to support flexibility in the system
clock frequency planning.

Attachments

    Outcomes