Can the AD9255 LVDS outputs drive signals over longer PCB trace?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can the AD9255 LVDS outputs drive signals over longer PCB trace, across
connectors, to another card (ADC is the last component in the signal chain on
the analog board before the signal goes to the FPGA on the digital board). Or
is a buffer required?

 

The LVDS interface is robust, and no buffer should be required, assuming that
the LVDS output traces are 100 Ohms Characteristic Impedance. For the CMOS
outputs, the load capacitance should be minimised and a buffer would probably
be required unless the trace length to the FPGS is very short.

Attachments

    Outcomes