When does the AD9249 require a digital reset after initial power-up?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

When does the AD9249 require a digital reset after initial power-up?

 

When powered on, the AD9249 goes into an initialization phase where an internal
state machine sets up the biases and the registers for proper operation. During
the initialization process the AD9249 needs a stable clock. If the ADC clock
source is not present or not stable during ADC power-up, it will disrupt the
state machine and cause the ADC to startup in an unknown state. In order to
correct this, an initialization sequence will need to be re-invoked after the
ADC clock is stable. This is done by issuing a DIGITAL RESET.

Attachments

    Outcomes