Input resistance for AD9231

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

What is input resistance of the analog input for AD9231? Only the input
capacitance is given in the datasheet.

 

The input series resistance of AD9231 in track-mode is about 30 Ohms. Track
mode is where most customers will be concerned with the input impedance. You
can find more information in the S-parameter data file which is available on
the AD9231 product webpage, under the Evaluation Boards & Kits link.

Outcomes