AD9129 - Compatible data generator ad9129

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

AD9129: Is there a data generator compatible with these devices?

 

Yes, ADI’s Data Pattern Generator (DPG) is a bench-top instrument for driving
vectors into Analog Devices' high-speed Digital-to-Analog converters. The DPG
connects to a PC over USB, and allows a user to download a vector from their PC
into the DPG’s internal memory. Once downloaded, the vector can be streamed-out
to the attached AD9129-EBZ evaluation board at the full data rate. This allows
for rapid evaluation of the DAC with both generic and custom-generated test
data.

Attachments

    Outcomes