Some soldered jumpers on the AD9122 Evalboard are not as per default settings mentioned in User Guide

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Some soldered jumpers on the AD9122 Evalboard are not as per default settings
mentioned in User Guide

 

Yes, there is an error in the User Guide (page 4).

The AD9122-M5375-EBZ and the AD9122-M5372-EBZ Evalboard User Guide states JP17
JP6 and JP4 and JP5 (pins 1&2)are connected by default (i.e. Figure 4(a)).
However, these jumpers are connected (pins2&3) by default according to 4(b).
The User Guide referred to is below:
ftp://ftp.analog.com/pub/HSSP_SW/HSCDAC/Documents/AD9122/AD9122%20Evaluation%20B
oard%20Quick%20Start%
20Guide.pdf

complete Documentation - Gerber Files, schmeatic etc...
ftp://ftp.analog.com/pub/HSSP_SW/HSCDAC/Documents/AD9122/

Attachments

    Outcomes