AD8611: Overdrive

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

in the ad8611 data sheet you are refering to "overdrive".
What is overdrive ?

 

Overdrive in a comparator is the difference in voltage between the + and -
inputs. If the threshhold is set at 2.5V, connected to the -ve input, and the
+ve input is a square wave which switches between 2.3V and 2.6V then the
overdrive is 0.1V for a rising edge input and 0.2V for a falling edge input.
Overdrive has an effect on the propagation delay of the comparator, as shown in
figure 2 of the datasheet.

Attachments

    Outcomes