AD8551 / AD8552 / AD8554: typo in datasheet Rev D figure 68

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

In figure 68 of AD8551 / AD8552 / AD8554 datasheet Rev D the part shown part in
the circuit is AD8552 and not AD8551. This is the conclusion of comparing the
figure with the pin configuration on page 1. The part in the circuit should be
AD8551.

 

Yes, in figure 68, the part in the circuit should be AD8551.  This will be
corrected at the next revision of this datasheet.

Attachments

    Outcomes