AD8515: Die size

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Are these dies AD8515 and OP284CHIPS smaller than 1 x 1 mm²? That would be an
absolute max for us.

 

1. The OP284CHIPS has a die size of 1.620 mm x 2.301 mm.
2. The AD8515 has a die size of 0.660 mm x 0.920 mm.

Therefore only the AD8515 would be smaller than 1x1 mm² as a bare die.

Attachments

    Outcomes