AD8476 - Stand-out performance specification

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What are considered to be the stand-out performance specifications of the
AD8476?

 

The AD8476 is extremely low power for an amplifier with its driving
capabilities. Furthermore, few fully-differential amplifiers have integrated
resistors, which allow AD8476 to guarantee very small gain error and
common-mode error. Also of note are the distortion performance and low voltage
offset and drift, which enable high dc precision. Applications with some
front-end gain will find that the noise performance is more than sufficient and
the power savings and  either single-ended to differential conversion or
input-to-output common-mode shift are very valuable.

Attachments

    Outcomes