AD8381: Temperature range

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

We are using the AD8381 chip in our system, and want to run it at -25°C.
As this chip is specified to 0°C, what happens if we make it run at -25°C?
There is no industrial range at such temperature?


The AD8381 is specified for commercial temperature range (0C to 70C). This is
the range of temperature over which the performance specifications in the
datasheet have been tested. We cannot guarantee that the device will meet these
specifications outside this temperature range.