AD8347 Demodulator Reference

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

The Base Band inputs IAIN, QAIN and detectors VDT1/VDT2 should be biased with
Vref (1V). When biasing these pins from another source which is also ~1V, I see
a failure in the AGC loop, it gets stuck at the minimum gain (VAGC = 3V).
What could be the cause of this strange behavior?

 

The internal VREF is very well controlled and your applied voltage can never be
as quite or clean as the chip’s band gap voltage.  The mixer AGC output level
is only 24 mVppk therefore if there is any noise or offset on the your applied
voltage then the AGC will be set to the minimum as you are observing.  Refer to
Figure 34.  You will need to use the chip’s internal VREF for the application
to work properly.

Attachments

    Outcomes