The AD8338 is consuming more than 3mA with very high, or very low gains

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

The AD8338 is consuming more than 3mA with very high, or very low gains

 

The AD8338’s unique architecture provides good gain at low currents at the
center of the gain range. As the gain deviates away from mid-gain (VGAIN=0.6V),
current consumption goes up. At the extreme ends, the device should not consume
more than 8mA.

Attachments

    Outcomes