AD8319: frequency range

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

For the design requirement of our project, the AD8319 needs to work in high
frequency band, such as 10GHz and 12GHz. From its datasheet, AD8319 can afford
the frequency of 10GHz use. I am not sure whether AD8319 could work in the
frequency of 12GHz. Could you please give some comments on the use of AD8319 in
frequency of 10GHz and 12GHz?

 

I have some data for the AD8317 at 11.7 GHz. The AD8317 is identical in
construction to the AD8319. The difference is the dynamic range of the AD8319
is slightly less. The attached data is at the edge of highest frequency the
part will operate at.
(Our parts are only guaranteed to operate up to the specifications provided in
the datasheet).

Attachments

Outcomes