AD8304: online tool intercept current.

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

The customer who is using AD8304 and the online tool to test their circuits. I
would like to confirm with you that if the Intercept value mentioned in the
online tool should be fixed to 1e-10A, that is 100pA. And if the Iz mentioned
in the datasheet is different from the Intercept current. How is the
relationship between the two things?

 

It is at 100pA, the standard intercept current.  However, you can change the
intercept current with the choice of external resistors, please see page 11 in
the datasheet. Also here is a spreadsheet in the attachment that may help more
than the online tool.

Attachments

Outcomes