AD8221 Input Bias Current

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

How did you come up with the 100GOhm specification for input bias current for
AD8221?

 

Essentially, it is the change in voltage at the input divided by the change in
input bias current.

Delta Vcm/ Delta Ib = Input Impedance.

See Figure 9: Ibias vs. CMV in the AD8221 data sheet.

We see we go from 0V to 10V and there is a 20pA change. That is 500GOhms. We
specify 100GOhms because it is a nice number. It will never be 100GOhms or
less. The input impedance will be larger than 100GOhms, but it is an easy
number to remember so we just put that down on the data sheet.

Attachments

    Outcomes