AD8211: Do I need to add a clamp diode to the AD8211 like DS high side current sensor section said?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Do I need to add a clamp diode to the AD8211 like DS high side current sensor
section said?

 

If the common mode voltage is 28V, and will not go above 68V, then a diiode
will not be necessary.

Attachments

    Outcomes