AD8138S: absolute maximum rating of  supply voltage

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I have a question to the absolute maximum ratings of AD8138S. When using the
AD8138S with a +/-5V supply everything is clear from the data sheet. The
absolute maximum rating is +-5.5V for the supply voltages. The point that in
not fully clear is when the AD8138S is operated from 0V to +5V single supply.
What is the absolute maximum rating in this case?

 

The positive supply can go as high as 11V, which is ok with the absolute max.
rating of +Vs to -Vs <= 11V.

Attachments

    Outcomes