AD8130: Power Dissipation Capacitance (Cpd) spec

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

We are using Analog devices component in our design. We need few component
parameters for our reliability analysis. We need Input Capacitance (Cin) and
Power Dissipation Capacitance (Cpd) for the component “AD8130”.

 

The Cin of AD8130 is 3pF(differential) and 4pF(common mode). Cpd is a
specification that is specific to the dynamic power consumption in CMOS logic
circuits, and is not directly applicable to our amplifiers.  This is why it is
not specified on any of our data sheets.

Attachments

    Outcomes