FAQ: Why would I choose to use DDS for synthesizing a signal rather than a PLL?

Document created by JLKeip Employee on Mar 12, 2010Last modified by AndyR on Jan 31, 2012
Version 2Show Document
  • View in full screen mode

Q.

Why would I choose to use DDS for synthesizing a signal rather than a PLL?

 

-----------------------------------------------------------------------------------------------------------------------------

A.

Let me start with a basic comparison between the two, but keep in mind this can change over time.

 

In general, it is fair to say that DDS technology provides some specific advantages:  dynamic frequency and phase control is relatively easy, and is not prone to ringing or settling, so if you need to do any sweeping or hopping, DDS is a good option to start.  DDS also provides much finer tuning resolution than even a fractional N PLL can provide.  The digital nature of the DDS also makes digital synthesis more repeatable.

 

Conversely PLL technology offers other benefits:  Generally speaking it is less expensive and less power hungry than DDS technology.  Perhaps most importantly, you have the ability to 'upconvert' your input frequency, whereas with the DDS is a Nyquist system, and limited to providing outputs that are <50% of the sampling clock frequency that is used.

 

But if you look beyond the surface, you 'll find a whole lot of softening of these boundaries.  For example:  There exist both 'ping pong' and 'fast hopping' PLLs on the market (including products from ADI) which close the gap in terms of their ability to provide frequency and even phase agile outputs.  Fractional N PLLs help close the gap on timing resolution for that matter.  Conversely, ADI has also closed the gap for DDS products in some cases.  Specifically worth noting is the AD9913, which significantly closes the gap both in power and in cost to PLLs.  ADI's DDS portfolio includes many products with reference clock PLLs on board, allowing customers to upconvert their reference clock before dividing down through the DDS, meaning the output can now be a higher frequency than the reference - note is is also possible to bandpass filter a DDS output isolating a Super Nyquist image to obtain an output frequency that is higher than the reference frequency source provided.

 

And taking it a step further, where fractional N PLLs closed the gap in terms of frequency granularity, the Programmable Modulus mode implemented in the AD9913 (and eventually most future DDS devices), widens that gap back up.

Attachments

    Outcomes