Common-mode range requirement for the AD7961?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the common-mode range requirement for the AD7961?

 

The AD7961 common-mode input voltage (VCM) range is half of the external
reference voltage used. For example, if the 5V external reference voltage is
used, the VCM would be 2.5V in this case.

Attachments

    Outcomes