What power supplies does the AD7961 require? Does it power down?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What power supplies does the AD7961 require? Does it power down?

 

The AD7961 operates from 1.8V and 5V supplies (VDD1 = +5V, VDD2 = +1.8V, VIO =
+1.8V), dissipating only 39 mW at 5-MSPS when converting in self-clocked mode.
The power dissipation scales linearly with throughput. When powering up the
AD7961 device, first apply 1.8 V (VDD2, VIO) to the device, then ramp 5 V
(VDD1) and apply an external reference voltage. Apply the analog inputs last.

The AD7961 powers down when EN3 to EN0 = X000 and operates in snooze mode when
EN3 to EN0 = XX11 using the correct reference choice.

Refer to CN-277 or UG-581 for complete information on how to generate the
required supplies for the AD7961.

Attachments

    Outcomes