AD7864: Chip Select Inputs

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Other inputs on the AD7864 (#STBY, #WR and Chip Select Inputs SL1 & SL2) are
going to be pulled high via pull-up resistors. Do these lines need to be pulled
high to the +3.3V supply or to the main +5V supply (DVDD)?


These can be pulled to the 5V supply, through pullups.