Will the AD7793 ADC continue to sample when the CS is disabled?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Will the AD7793 ADC continue to sample when the CS is disabled?

 

In the sigma delta converter CS only influences the serial interface and the
serial interface is independent of the sampling process. Conversion is
controlled solely by the internal clock, the user only has control of reading
the data.

For more information on the operation of a sigma delta converter see following
resources:

Chapter 3.3 (page 109) of data Conveter seminar:
http://www.analog.com/library/analogDialogue/archives/39-06/data_conversion_hand
book.html

FAQ on AD779x sigma delta ADCs:
http://www.analog.com/static/imported-files/faqs/AD779x_FAQ_Instru_Conv.pdf

Attachments

    Outcomes