EVAL-AD7746EBZ Evaluation Board Software for Matlab Connection

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

I would like to create my own application in LabWindows based on AD7746
Evaluation Board Software with capacitive humidity sensor, therefore could I
ask you for source code of AD7746 Evaluation Board
Software ? I have problem with communication protocol used in EVAL-AD7746EBZ.


The evaluation system contains our CDC component, which we want the customers
to evaluate and to which we are, of course, prepared to provide full support

The evaluation system also includes a third party (Cypress) USB microcontroller
in order to allow connection to PC via the today's most common USB interface.
We provide user interface software for the PC to use the evaluation setup in
order to perform data acquisition and basic analysis.
We cannot support a connection of the Cypress uC via the USB interface to
customer specific system, a system which is to us unknown and unspecified. We
have only limited knowledge of the Cypress controller and drivers ourselves,
the DLL that we use on PC are very little documented. We cannot provide support
for that third party component in our evaluation system.

However it is possible to make some Labview example code available. This
Labview example code uses all components required to access the CDC on the
evaluation board via Labview on the PC. The overall functionality can be
adapted by the customer.

(Please see attached labview example code).