AD7730_calibration coefficient

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

We have a customer who would like to know how does the Gain Calibration
Register influences the conversion results in AD7730. He want to get the
calculation formula.


In unipolar mode, the relationship is
Data = [(0.75 × VIN × Gain/VREF) × (2**23) – (Offset_Reg – 0x800000)] ×
Full_Scale_Reg/0x400000 × 2

In bipolar mode, the relationship is
Data = [(0.75 × VIN × PGA_Gain/VREF) × (2**23) – (Offset_Reg – 0x800000)] ×
Full_Scale_Reg/0x400000 + 0x800000

Data = digital conversion
VIN = applied analog input voltage
Gain = PGA gain setting
VREF = reference voltage
Offset_Reg = value contained in the offset register
Full_Scale_Reg = value contained in the full-scale register
The nominal values of Offset_Reg is 0x800000 and of
Full_Scale_Reg is 0x555555.
The 0.75 number will vary slightly from part to part because of
manufacturing tolerances.

1 LSB of the offset register is equivalent to approximately 1.3 LSB of the data
register, assuming the nominal full-scale coefficients are present. The exact
value varies slightly from part to part, and the ratio changes if the
full-scale register coefficients are modified.
The exact ratio can be derived by dividing the value in the full-scale register
by 0x400000. This gives a value close to 1.33 with the nominal full-scale
coefficient of 0x555555. But if the full-scale register is modified by the
user, the ratio changes. This occurs since the offset removal is performed
before the gain scaling when the ADC is adjusting the converter output.
The full-scale register can be interpreted as a multiplication factor, whose
value equals (full-scale coefficient/0x400000.) Since the scaling is done after
the offset register is removed, the relative weight of an offset register LSB
is different to a data register LSB.
The nominal value of 1.3 for the gain scaling is because the input signal is
attenuated by 3/4 as part of the ADC conversion. A 4/3 scaling is then required
to digitally compensate for this. (This is normally transparent to the user;
it’s only when manipulating calibration values that this can become apparent.)

The signal flow can be viewed as
[Input Signal] -> [PGA] -> [Attenuation by 0.75] -> [ADC Conversion] ->
[Subtract Offset] -> [Scale by FS/0x400000] -> [Data Register]

If the system offset calibration is done using the ADC’s system zero-scale
calibration mode with the systems zero-scale point applied as input voltage,
then this scaling factor does not need to be accounted for, since the ADC
calibration routine will write the correct value into the offset register. It’s
only if calibrations are done using regular conversions (that is, a result is
written into the data register) that a scaling factor is required before
writing into the offset register.

For the full-scale coefficient or full-scale calibrations, it is a simple
scaling coefficient, so to increase the gain of the ADC by 10%, the full-scale
coefficient needs to be increased by 10%.