ad7745: Sensors with higher capacative range

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

They make humidiysensors with a capacitive output. Therefor, they have
interests in CDC as AD7745. But the nominal capacitance of their sensors is
180pF with a max. change of +-50pF, which is higher than the AD7745 can handle.


1) Connect a known fixed capacitor in series with the sensor. That would work
by equation C = C1 x C2 / (C1 + C2). This method results in a non-linear
relation between the sensor capacitance and the output data, but this can be
corrected in the host uC software. Also, the AD7746 input range might not be
fully used with implication of lower signal/noise ratio, but I believe the
AD7746 itself has enough resolution to keep the system resolution on required
level. My main concern would be how stable is the serial capacitor over
temperature and temperature compensation for that.

2) Reduce the excitation voltage. The AD7746 basically measures charge and
reducing the excitation voltage, proportionally higher capacitance can be