AD7606 throughput rate

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

The datasheet describes AD7606 as sampling at throughput rates up to 200
kSPS for all channels. It is not clear if this means 200 ksps for each of the 8
channels or if you
need to divide the 200 ksps by 8.

 

The core ADC inside the AD7606 is > 1 MSPS so this is shared across all 8
channels. The cycle time to have all 8 channels converted is 5 us (depending on
ser/par interface). So it is 200 ksps for each of the 8 channels(You do not
need to divide the 200 ksps by 8).
1 person found this helpful

Attachments

    Outcomes