Why do the AD7606 pins in the "Typical Connection Diagram" such as RANGE, /STDBY have resistors and what values should they be?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Why do pins RANGE, STBY, REFSEL, SER/PAR have resistors and what values should
these resistors have?


These pins are all digital input pins and the resistors act as
pull-up/pull-down resistors, in order to pull the logic inputs to the required
level. A value of 1Kohm should be enough for these resistors.