AD73360: Settling time when changing the PGA gain

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the setting amplification factor time from 0 dB to 38 dB, if chip work
with 3.3 volt?

 

The PGA is implemented by changing the sampling of the input signal, this is a
common PGA structure for most of our sigma delta converters, therefore the
response time of the PGA is not an issue. Changing from 0 to 38db, is
equivalent to a step change or a channel change at the input. The delay to o/p
can be obtained by looking at the group delay of the filter for the various
sampling rates on page 2 of the datasheet.

Attachments

    Outcomes