AD73322L: Frequency response

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I have a question relating to the operation of the AD73322L frequency response.

I am testing the device with Sine wave tones ranging across the voice band
between 300Hz and 3400Hz and
Am finding that with a sampling rate of 16Khz, I am getting a 25% reduction in
output at 3400 compared
To 300Hz.

Is this attenuation the correct operation of the device? I was expecting a flat
response.

Are there any setings in the registers which affect the frequency response?

I found that 8Khz sampling gave distortion to the wave at 3400Hz so increased
to 16Khz.

 

This is actually the correct or expected frequency response of the  device. It
uses a Sinc^3 filter to provide low group delay - however this filter response
is quite "soft" with roll-off in the pass band that continues into the
transition band.

If the device is being used with a DSP as is normally the case, a Sinc^3
compensation filter operating at 16 kHz with decimation to 8 kHz can provide a
flat response out to 3400 Hz and provides a sharp transition band.

The other alternative is the AD74111 which is a mono codec but has a more
traditional filter which gives flat pass band response and sharp transition
band.

Attachments

    Outcomes