AD7280 AD7280A - can the part work with 3 cells?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Would the AD7280 work with 3 cells if a cell has:

Nominal Voltage: 3.7V
Cut-Off Voltage: 2.7V
Continuos Current: 150.0A

3*2.7V=8.1V – which is 100mV above the 8V min – and this in general speaking


Yes, as soon as minimum voltage is above the AD7280 VDD min specification the
part will work.