Filter Options

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

There are a number of filter options.  Which one should I use?


The AD7176-2 has three filter options: Sinc5+Sinc1, Sinc3 and enhanced 50 & 60
Hz filters. The Sinc5+Sinc1 is most suited to multichannel applications where
fast multiplexing is required. The Sinc3 is best for single channel
applications running at lower output data rates. In applications where
rejection of 50 and 60 Hz is important the enhanced 50 & 60 Hz rejection
filters should be used as they provide better performance than the Sinc filters
and allow the user to trade off settling time or rejection to meet their
application needs. We provide a filter tool to help during design-in. See