AD7124-8 When single conversion mode is used, can   be taken high after the single conversion is initiated?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

AD7124-8 When single conversion mode is used, can   be taken high after the
single conversion is initiated?

 

The serial interface is independent of the sampling process. So, once the
single conversion is initiated, the AD7124-8 will power up and perform the
single conversion irrespective of the  polarity. So, the user can take  low,
initiate the single conversion and then take  high again. When the conversion
is complete,  can be taken low to read the conversion and another single
conversion can be started if required.
When  is taken high, the DOUT/ pin is tri-stated. Therefore, the DOUT/ pin will
not indicate the end of the conversion. The user can determine the end of the
conversion by reading the status register. Alternatively, the conversion time
could be timed out by the microcontroller clock.

Attachments

    Outcomes