AD7091: Can Vdrive be greater than Vdd

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can Vdrive be greater than Vdd?


Yes, Vdrive can be greater than Vdd. It should be noted that if the 1LSB INL
specification is important to the application then Vdrive should not exceed Vdd
by more than 0.7V. Also the performance limit for Vdd and Vdrive is 5.25V.