AD7091R MSB always 0 after each conversion

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Why after every conversion is the MSB of the conversion result always “0”?


If the communication timing is ok this is usually due to the time between the
/CONVST start  pulse going low and reading back the conversion. The conversion
time is 650ns maximum. If the result is read back before this time has elapsed
then it is possible that the MSB will be zero.

You can also use the BUSY indication feature to indicate when a conversion is
complete by having /CS low prior to the EOC point. This will take the SDO line
out of high impedance once a conversion completes and this can be detected by
the SPI master.