AD7091R ADC Input Levels

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can the ADC inputs exceed the reference voltage or go below ground?

 

The ADC inputs should not exceed the reference voltage or go below ground by
more than 0.3V
as this may result in the ADC being damaged. If this is a common condition then
schottky diodes should be used to protect the inputs and limit them to <0.3V.
The maximum input current to the analog input is +/-10mA.

Attachments

    Outcomes